This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Difference between 'unitTest' and 'pktRouterTest' of NWAL drivers

Other Parts Discussed in Thread: TCI6636K2H

Hi all,

I am using XTCIEVMK2X - TCI6636K2H EVM. 

Developing environment is: CCS ver  5.4.0.00091

MCSDK Packages: 3_00_01_12

I can see in the test folder of NWAL ( C:\ti\pdk_keystone2_3_00_01_12\packages\ti\drv\nwal\test), there are two folders. One is 'unitTest' and another one is 'pktRouterTest'.

Could you please provide the differences between these tests ? As its necessary for us to use some of APIs from these tests.

Thanks,

Rajanikanth.