This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SDK 1.1.0.3



Hi,

we are using SDK 1.1.0.3 Ethercat applictaion on earlier ICE_SCH version.

We are using below listed few GPIO's for other application in our design, But With new schematics ICE_SCH v2.0 GPIO's is observed to be used

Can any one help us out to undersatnd where they are used : As we are using the newer SDK 1.1.0.3  firmware with earlier version of ICE_SCH

GPIO0[14] , GPIO3[20], GPIO1[8] , GPIO0[0] , GPIO0[17]

6) GPIO1[9]

Is it being used in sync0Isr and Sync0task alone?

7) GPIO3[2]

Is it being used to indicte error led in LEDDriveACT0 function alone?

8) GPIO0[7]

FET switching, Is it being used in UTILsInitCpswIcssPorts alone?

9)GPIO0[16]

Is It being used LEDDriveRun alone?

 Regards,

Bindu