This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRM on linux-3.12.4 kernel for omap5-evm board

Hello,


I am trying to run 3.12.4 kernel on the omap5-evm board .

GIT REPO = git://git.ti.com/ti-linux-kernel/ti-linux-kernel.git

BRANCH = "ti-linux-3.12.y"

COMMIT = "9921cde9aa3f323d5a0e9e5207b7ad173652a89d"

Recipe: http://arago-project.org/git/projects/?p=meta-ti-glsdk.git;a=blob;f=recipes-kernel/linux/linux-ti-staging_3.12.bb;h=eaf0df25fb0724e8e70f079f55c08dd7c680ce79;hb=d17b707a9b25ef40bdc7a583491ca648c4462f67


By default in the omap2plus_defconfig DRM is not enabled. When is it expected that the kernel would have DRM support  ?


I did try to manually enable DRM on the kernel but wasn't able to run any of the drm sample applications on the board.

  • Hi  Abhijit,

    did you examine the following  link:

    http://arago-project.org/git/projects/?p=meta-ti-glsdk.git;a=commit;h=2144ae369a1554064809c1a432784e8c44705a9e

    You can also address the guys in the GLSDK forum they will probably  provide you with more up-to-date information.

    Regards,

    Boyko