This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DDR3 INTERFACE



HI ALL,

With respect to the DM8148 DDR III controller, in referencing the SPRS647B ( datasheet ) and the SPRUGZ8 ( Technical Reference Manual ), I am confused regarding the total memory size supported by the Dm8148.

Datasheet page 2 indicates 2GB total memory address space, where the TRM page 910, section 6.1.2, indicates 1GB toal memory address space.

I am using MT41K256M16HA-107 Micron DDR3(256MX16) , i need to achieve 1GB density, currently i am using TWO devices.

DM8148 having two channel , i have confusion on each channel need to be use or any one channel i can use to achieve 1GB(256MX16)

Regards,

Arun

MT41K256M16HA-107 IT:E
  • Hi Arun,

    ARUNA KUMAR K H said:
    SPRUGZ8 ( Technical Reference Manual )

    ARUNA KUMAR K H said:
    where the TRM page 910, section 6.1.2, indicates 1GB toal memory address space.

    The latest version of the DM814x TRM is SPRUGZ8E:

    http://www.ti.com/lit/ug/sprugz8e/sprugz8e.pdf

    section 6.1.2 Features does not state that DDR3 supports up to 1GB.

    Up to 8 2Gbit DDR3 devices can be used, totally 2GBytes.

    http://processors.wiki.ti.com/index.php/EZSDK_Memory_Map#Changing_Memory_Map_For_512MB_DM816x_Board

    In the default uboot program ( in file $(EZSDK_ROOT)/board-support/u-boot-<REL-TAG>/board/<ti8168 or ti8148>/ti/evm.c), 2GB physical memory is mapped using register 3 and 4.

    Following code programs the LISA registers for 2GB physical memory

    Best regards,
    Pavel

  • Dear Pavel,

    There is a two channel , Currently i am using DDR0 channel with 2 devices of X16. remain DDR1 channel i am not going to use.weather i need to add any pull up or pull down for unused DDR1 channel .

    Please give me a inputs.

    Thanks & Regards,

    Arun

  • Arun,

    You can refer to the below e2e thread:

    http://e2e.ti.com/support/arm/sitara_arm/f/791/t/278135.aspx

    It is for AM335x device, but recommendations are also valid for DM814x/AM387x device.

    Also you can have a look in the DM814x datasheet, sections 4.4 Handling Unused Pins, 4.5.1 Pullup/Pulldown Resistors and 8.13.4.2 DDR3 Routing Specifications.


    And the below for the software side:

    http://processors.wiki.ti.com/index.php/TI814x-DDR3-Init-U-Boot#FAQ

    Best regards,
    Pavel