This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Difference between ES1.0 and ES2.0

Hi,

What is the difference between OMAP5 ES2.0 and OMAP5 ES1.0 in terms of graphics/video capabilities or difference which affects graphics and video performance?

Thanks & Regards,

Vikas

  • Hello Vikas,

    In a nutshell the changes in the graphics/video modules in OMAP5, between ES1.0 & ES2.0 are the following:

    IVA-HD - no change between the two revisions of the device.

    Cortex M4 - IPU Subsystem - no change between the revisions of the device.

    ISS - the following changes are made in ES2.0:
      - The maximum data rate on the CSI2 interfaces (CSI2_A, CSI2_B and CSI2_C) is increased from 1 Gbps to 1.5 Gpbs per lane.

     - The frequency of RXBYTECLKHS_A, RXBYTECLKHS_B and RXBYTECLKHS_C byte clocks provided by corresponding CSI_PHYs is increased from 125 MHz to 187.5 MHz for OPP_NOM 

    OPP_LOW is not supported for VD_CORE in OMAP543x Silicon Revision 2.0

    The TCTRL cam_strobe and cam_shutter signals are exported on a second pair of alternative device pads.

    CSI3 interface (CAL, MIPI UNIPRO2 and MIPI MPHY) is not supported in OMAP543x Silicon Revision 2.0.

    ISP & SIMCOP remain unchanged between the two chip revisions.

    DSS Subsystem:

    • OPP_LOW removed as not supported at VD_CORE.
    • F_CLK increased from 200 to 209.25MHz at OPP_NOM.
    • LCDx_CLK increased from 200 to 209.25MHz at 100% OPP_NOM
    • DSI1_x_CLK increased from 200 to 209.25MHz at 100% OPP_NOM
    • DSS_DISPC_LDCx_PCLK increased from 200 to 209.25MHz at OPP_NOM.
    • DSI1_x_TX_BYTECLKHS increased from 125 to 150MHz at OPP_NOM.
    • Due to the above the max DSI resulution supported changed to 2048x1536 @ 60 FPS with 24bpp

    - DISPC:

      The following new features associated with the DISPC DMA engine are added:
    • Microsoft Flip-Immediate feature (on-the-fly Base address update) (GFX, VID1, VID2 and VID3
    pipelines). List of registers impacted:
    – DISPC_BA0_FLIPIMMEDIATE_EN
    – DISPC_IRQENABLE[31] FLIPIMMEDIATEDONE_EN
    – DISPC_IRQSTATUS[31] FLIPIMMEDIATEDONE_IRQ
    • New support for MFLAG mechanism for dynamic increase of the priority of real time data traffic for the
    GFX, VID1, VID2, VID3 and WB pipelines. List of registers impacted:
    – DISPC_GLOBAL_MFLAG_ATTRIBUTE
    – DISPC_GFX_MFLAG_THRESHOLD
    – DISPC_VID1_MFLAG_THRESHOLD

    – DISPC_VID2_MFLAG_THRESHOLD
    – DISPC_VID3_MFLAG_THRESHOLD
    – DISPC_WB_MFLAG_THRESHOLD

    • Force 1D access in tiled mode functionality added. List of registers impacted:
    – DISPC_GFX_ATTRIBUTES[16] FORCE1DTILEDMODE
    – DISPC_VID1_ATTRIBUTES[20] FORCE1DTILEDMODE
    – DISPC_VID2_ATTRIBUTES[20] FORCE1DTILEDMODE
    – DISPC_VID3_ATTRIBUTES[20] FORCE1DTILEDMODE
    – DISPC_WB_ATTRIBUTES[20] FORCE1DTILEDMODE

    System performance optimization for 3D rendering via the following formats:
    • Line alternative format (ref: HDMI Specification 1.4a)
    – Lines from the left and the right frames are interleaved alternatively on the screen to produce a 3D
    image.
    – Required also to support interleaving column-wise to support all possible screen orientations.
    • DISPC_CONFIG1
    • DISPC_CONFIG2
    • DISPC_CONFIG3
    • Frame Packing format (ref: HDMI Specification 1.4a)
    – The left and the right frame are sent one after the other.
    – To enable multiple 3D displays with 3D GUI overlay, it is required to use a single pipe (graphics or
    video) to fetch both left and right frames.
    • DISPC_GFX_ATTRIBUTES[10] FRAMEPACKINGMODE
    • DISPC_VID1_ATTRIBUTES[8] FRAMEPACKINGMODE
    • DISPC_VID2_ATTRIBUTES[8] FRAMEPACKINGMODE
    • DISPC_VID3_ATTRIBUTES[8] FRAMEPACKINGMODE
    • DISPC_GFX_POSITION2
    • DISPC_VID1_POSITION2
    • DISPC_VID2_POSITION2
    • DISPC_VID3_POSITION2
    • DLP 3D TV format
    – The left and the right frame are interleaved in a checker board pattern.
    – The left and the right frames are sub-sampled by 2 along the diagonal to preserve vertical and
    horizontal resolution.
    • DISPC_GFX_ATTRIBUTES[20:18] SUBSAMPLINGPATTERN
    • DISPC_VID1_ATTRIBUTES2[11:9] SUBSAMPLINGPATTERN
    • DISPC_VID2_ATTRIBUTES2[11:9] SUBSAMPLINGPATTERN
    • DISPC_VID3_ATTRIBUTES2[11:9] SUBSAMPLINGPATTERN
    • BGRA32-8888 format added. List of registers impacted:
    – DISPC_GFX_ATTRIBUTES[4:1] FORMAT
    – DISPC_VID1_ATTRIBUTES[4:1] FORMAT
    – DISPC_VID2_ATTRIBUTES[4:1] FORMAT
    – DISPC_VID3_ATTRIBUTES[4:1] FORMAT
    – DISPC_WB_ATTRIBUTES[4:1] FORMAT

    - MIPI DSI

    • Maximum data rate increased from 1000 to 1255.5 Mbps per data pair for four-data lane configuration
    • PHY clock incresed from 500 to 627.75MHz at OPP_NOM.

    3D Accelerator GPU Subsystem: remains unchanged between the two revisions.

    2D Graphics Accelerator: BB2D subsystem is introduced for the first time in OMAP5 ES2.0

    For a complete difference between chip revisions please contact your TI representative. There is a delta document available under NDA agreement.

    Best Regards,

    Yordan

  • Thanks Yordan for information. There is one change in 3D GPU i.e. SGX core revision changed from 105 to 116 which is suggested by following post.

    http://e2e.ti.com/support/omap/f/885/p/263519/1109899.aspx#1109899

    Thanks & Regards,

    Vikas