Hi Everyone,
I have got a project that using Concerto F28M35H52C1 board and TIRTOS. The project aims to download a file which is around 27MB from the SD card through http and IP. The webpage is shown in the figure below. When "download" is pressed, file starts to be downloaded from the SD card. However, downloading process always stops at around 5.6MB which is not accomplished. Can anyone help to solve this problem? The CCS code and files on the SD card are attached. Please try it. The steps are listed as below.
1. Unzip the files and copy the two files (index.html and Albatern.csv) into the SD card.
2. Change the program mac setting to your MAC address of the Concerto.
3. After running the program, just type in the IP address: 192.168.2.10 (I am using Firefox)
Many Thanks in Advance!
Ben