This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x low GPIO hysteresis

Hi engineers

We are using GPIO inputs on AM3358ZCZ, using inputs GPIO3_18 to GPIO3_21 (3.3V domain).
According to the data sheet (sprs717f page 93) the hysteresis voltage shall be between 0.265V to 0.440V for VDDSHVx=3.3V.
When we measure we have a hysteresis between 172mV to 197mV.
On GPIO3_20 we have as low as 38mV.

Q: Why these low hysteresis voltages, they are 100mV lower than the spec?

Q: Why does GPIO3_20 deviate from the other, having only 38mV hysteresis?

Thanks in advance!