This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

source code of ROM Ethernet bootloader - K2H

Hi all,

I am using XTCIEVMK2X EVM. 

Developing environment is: CCS ver  5.4.0.00091; MCSDK Packages: 3_00_01_12

Where can I get the source code of  ROM Ethernet bootloader for this EVM ?

Thanks in advance.

Thanks,

Rajanikanth.

  • Hi all,

    Can you please let me know,  RBL code written for 'C6678 KeyStone devices' is still valid for K2H devices ?

    or

    Do I need to use the separate bootloader code of K2H devices ?

    Please let me know where can I get the source code of  Ethernet ROM bootloader for the EVM - XTCIEVMK2X.

     

    Thanks in advance.

    Thanks,

    Rajanikanth.

  • Hi all,

    In addition to the above info, I am trying to use 'DSP Ethernet boot mode' on XTCIEVMK2X EVM.

    By considering this point, please let me know,   do I need to use the separate bootloader code for K2H EVM or still I can use bootloader code of  'C6678 KeyStone devices' ?

    Thanks,

    Rajanikanth.

  • Hi Rajnikanth,

    We have not released the ROM source code for K2H. I am checking internally with the software teams as to when this can be made available. DSP boot of K2H is similar to Keystone I devices, can you please specify the issues you are facing while trying to boot DSP over ethernet. On the EVM, there is no need for an IBL as was the case with the C6678 EVM. 

    Regards,

    Rahul

  • Hi Rahul,

    Thanks for your reply.

    Facing problem while running bootloader code on K2H platform.  Earlier we successfully  able to boot  on C6678 device and at present we are using the same (C6678's) RBL code on K2H platform.

    So, just suspecting will C6678's RBL code will valid on k2H platform or not ?

    I will specify the exact issue what we are facing.

    Thanks & Regards,

    Rajanikanth.