As our C6657 core supply design was based on the latest available hardware documentation back in 2012 (ie. Figs 17&18 of SPRABI2B, March 2012), the UCD side of the VID signals are not pulled to 3.3V.
1. Is the lockout mechanism on the UCD9222 a valid approach to dealing with misbehaving VID inputs early in the power cycle?
2. If so, TI documentation is not clear on the timing relationship between valid power rails (specifically CVDD and I/O supplies), reset, and the C6657 driving its VID outputs. Specifically what is the timing relationship?