This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Boot problem for TiDSP C6452



Hi,

i am getting a boot problem when we try to boot our C6452 DSP. its quite strange that it does not happen every time and also with same DSP. it occures some time only with some DSP's. And also we are using different .out files others are working fine. only we have problem with one .out file.

i made a temporary work around for this problem if booting fails, booting is done upto 5 iterations until it is successful. At the beginning it seems working, when second time DSP is booted with the .outfile(first time fails in this case) but now it is also failing all 5 times.

Do any one have idea why it behaves strange like this? perfectly booting lot of times at the beginning itself,some times second times(i.e second iteration) some times working completely not(upto 5 iterations).

do some one has any idea?Why DSP behaves strangely like this?

Thanks,

Ramana.