Hi All,
I am trying to work on beagle board OTG with sdk 06.00.00.
The device is working either as a HOST or a DEVICE
The issue is once hdrc mode is changed to a_idle state it never returns to b_idle or b_ peripheral state and
i need a reboot to make it return to b_idle .
cat /sys/devices/platform/omap/musb-omap2430/musb-hdrc/mode is b_idle at boot up. And when i
connect OTG cable the mode changes to a_idle and never returns to b_idle on disconnecting the OTG cable . I
have connected the board to PC by a MIniB usb Cable but the mode remails at a_idle. Is there any kernel patch
available for this issue? Any one point me how to solve this issue.
Regards,
Dibin