This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Android support for Jacinto 6



Hi,

   I am working on Jacinto 6 evm dra7xx board. I am looking to flash Android OS image on this board. Could you provide pointers from where to get this pre-built image ...

  • Hello,

    There are two releases of Android for Jacinto 6:
    6AJ.1.1 : http://omappedia.org/wiki/6AJ.1.1_Release_Notes#Using_the_Prebuilt_Release_Image

    6AJ.1.2 : http://omappedia.org/wiki/6AJ.1.2_Release_Notes#Using_the_Prebuilt_Release_Image


    You should click on the link embedded in the statement:
    " The prebuilt release image can be obtained from here"

    Best Regards,

    Yordan

  • The repositories are:

    http://software-dl.ti.com/omap/jacinto6/JACINTO6-EVM/6AJ_1_1_Release/index_FDS.html

    and

    http://software-dl.ti.com/omap/jacinto6/JACINTO6-EVM/6AJ_1_2_Release/index_FDS.html