Other Parts Discussed in Thread: TSC2004
Hello,
I am connecting GIO8 of DM365 to a pin of another IC which is always toggling (seen in CRO).Also I am able to read the state of GIO8 in the program.But I want to configure GIO8 as interrupt.I have registered interrupt , but the printk messages in the handler is not getting printed.
uname -a returns Linux DM365_IPNC 2.6.18_pro500-davinci_IPNC_DM365_2.0.0
The following is the code used.
gpio_request(8, "tsc2004-irq");
temp = __raw_readl(pinmux3);
temp = temp & 0xFFFFFF7F;
__raw_writel(temp, pinmux3);
gpio_direction_input(8);
temp = davinci_readl(DM365_ARM_INTMUX);
temp &= 0xffffbfff;
davinci_writel(temp , DM365_ARM_INTMUX);
data->irq = gpio_to_irq(8);
if (request_irq(data->irq , tsc2004_irq, IRQF_TRIGGER_FALLING, "tsc2004" , NULL)) {
err = -EBUSY;
goto exit_free;
}
mdelay(10000);
static irqreturn_t tsc2004_irq(int irq, void *handle,struct pt_regs *regs) //ISR
{
printk("\n ------------------------ in ISR -------------------------------\n");
return IRQ_HANDLED;
}
# cat /proc/interrupts
CPU0
0: 0 AINTC csl
1: 0 AINTC csl
2: 0 AINTC csl
3: 0 AINTC csl
4: 0 AINTC csl
5: 0 AINTC csl
6: 0 AINTC csl
8: 1015 AINTC davinci_osd
16: 0 AINTC EDMA Completion
17: 0 AINTC EDMA CC Error
18: 0 AINTC EDMA TC0 Error
19: 0 AINTC EDMA TC1 Error
26: 411 AINTC davinci-mmc
29: 0 AINTC rtc0
32: 191917 AINTC clockevent
33: 1 AINTC free-run counter
39: 21 AINTC i2c_davinci
40: 3412 AINTC serial
42: 0 AINTC dm_spi
61: 0 AINTC EDMA TC2 Error
62: 0 AINTC EDMA TC3 Error
72: 0 GPIO tsc2004
Err: 0
SHould I add anything in addition to the above code ?
As soon as I load this module I am expecting printk messages in the handler (GIO8 toggling in CRO).But I couldn't find any messages in dmesg.Can some one help me out to figure it out ?
Regards,
Nizar