This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Clock inputs to Keystone 2 devices through clock buffer

Hello,

I am using CDCLVD110 clock buffer to provide cock inputs to TCI6638 SoC and C6678 DSP. As per datasheet of CDCLVD110 output capacitance of its LVDS drivers is 3pF whereas datasheet of keystone devices don't specify input capacitance at LVDS clock input pins. Can I connect CDCLVD110 to Keystone devices with DC blocking capacitors or should decide based on input capacitance of keystone devices?

Regards

Sachin