Other Parts Discussed in Thread: AM3359
Hi
We are using ICE AM3359 , SDK 1.1.0.3 Ethercat application
We are trying to combine both EtherCAT and Web sever into single application
We assume it is possible to use EoE (Ethernet over EtherCAT) to send Ethernet packets to slave using EtherCAT network and LwIP application run on top of EoE layer of EtherCAT.
f we make use of EOE for Web server application :
1)Execution of EtherCAT application and the EtherCAT Master connectivity with slave is needed?
2)If the EtherCAT Master slave connectivity is needed then EOE Communication can happen on other Ethernet PORT ( Not the one communicating with EtherCAT Master) or the same Ethernet PORT (One used by EtherCAT master).
Regards,
Bindu