Hello,
I have an confirmation about DM36x USB port.
It has two modes, Transparent mode and RNDIS mode.
When the DM36x is the RNDIS mode, receiving zero byte packet means end of complete transfer.
And it always generates the interrupt. Is it correct?
I would like to use DM36x USB port as host and connect to USB Camera(UVC) device.
While the USB camera is blanking time, it sends zero byte data to DM36x USB.
Can I use RNDIS mode in this case?
Best regards, RY