Other Parts Discussed in Thread: TMS320VC5510A
Hi,
We are currently running a TMS320VC5510A DSP on our custom target hardware platform. We have recently attempted to upgraded from v3.3 of Code Composer Studio to CCS 4.0 and I'm getting the following unexpected error each time I halt the Target DSP (DSP) when running from the USB-based XDS510 emulator:
C55xx_0: Trouble Halting Target CPU: Error 0x20010000/ -2011 Severe Error during: RTDX, An internal error occurred in which an illegal action (0xC0C1C2C3) was requested while disconnected
We are not even using RTDX and it's not clear to me how to determine if it was incorrectly enabled when the CCS 4.0 migration wizard converted my CCS v3.3 project. Has anyone else seen this error? How can I determine if RTDX is enabled and if it is, disable it
Any help would be appreciated.
Thanks,
Brad S.