Hi,
I have a 8168EVM with IO card, and I am using dvrrdk3.0. I have problems to use TVP7002 to capture videos.
What changes should I make to run dvrrdk3.0 on this EVM?
Regards
Michael
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have a 8168EVM with IO card, and I am using dvrrdk3.0. I have problems to use TVP7002 to capture videos.
What changes should I make to run dvrrdk3.0 on this EVM?
Regards
Michael
DVRRDK doesn't support EVM+XIO daughter card so there is some porting effort.
First migrate to DVRRDK 4.1 and then refer this most where EVM+XIO daughter card is used to capture 720P using TVP7002
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/p/304675/1064197.aspx#1064197
You should disable configuration of external video decoder on capture side and disable offchip HDMI configuration on display side as these are daughter card specific. You will have to do the relevant TVP configuration via i2c from your application