Other Parts Discussed in Thread: AM3359
I have an issue with an unusually long latency of ~60us for enabling/disabling DMTimer on AM335x.
I originally posted this issue on the StarterWare forum: http://e2e.ti.com/support/embedded/starterware/f/790/t/314982.aspx
This issue may not necessarily be caused by the StarterWare, so I am posting it again here.
--------------------------------------------------------------------------------------------------------------------
Hello,
I have a board with the AM3359 processor, running at 600 MHz.
I am using CCS v5.4, SYS/BIOS 6.35.1.29, and the Sitara SYS/BIOS Industrial SDK v1.1.0.1.
I am using the DMTimer peripheral for my application.
More specifically, I am using DMTimer3 in one-shot mode, and I start the timer roughly every 500us.
While using the RTA Execution Graph, I noticed that the ISR for the DMTimer takes an unusually long time. After commenting out "DMTimerDisable(SOC_DMTIMER_3_REGs)" I noticed that the execution time improved by 60us, indicating that disabling the DMTimer was taking 60us. The CPU Load of my application also fell from 55% to 45% when I commented out that one line of code. "DMTimerEnable(SOC_DMTIMER_3_REGs)" also takes 60us. Clearly, something is very wrong. A 600 MHz processor should not take 60us to write to a register.
I had some difficuly getting the SYS/BIOS HAL API and the StarterWare from the SYS/BIOS Industrial SDK to work well together when configuring the DMTimer peripheral. My previous difficulties with the configuration are discribed in this post: http://e2e.ti.com/support/arm/sitara_arm/f/791/t/194331.aspx
I was finally able to get the timer configured, and it "works", but apparently there may still be some issues, as indicated by the extremely long time it takes to enable/disable the DMTimer.
I would appreciate any information that might help to diagnose why toggling the DMTimer peripheral is so sluggish.
Thanks.