Other Parts Discussed in Thread: OMAP-L138
Hi,
I am using document as example: http://software-dl.ti.com/trainingTTO/trainingTTO_public_sw/bios/BIOS_14b_Flash.pdf
I am using the following:
Board: EVMC6748 (I am using the TMS320C6748 DSP).
I am connected using the ethernet port to my router.
ccs: 5.4.0.00091
bios: 6_35_01_29
pspdrivers: 01_30_01
nsp: nsp_1_10_02_09
ndk: ndk_2_22_03_20
xdctools: 3_25_00_48
xgconf
---
When running the SPI Writter I chose N and then the bin file I created according the document.
1) After about 2 minutes only I get message "INFO: File read complete."
2) I waited additional 5 min, nothing else appears....
Any idea?
Thanks in advance!!!