Hi,
When using the McBSP in Clock Stop Mode (SPI), the packet length can be 8 -32 bits. If the packet length is set for 8 bits, and since the 5509A doesn't allow byte-aligned transfers, which half of the word gets sent or received (MSB's or LSB's)? The documentation seems to indicate the LSB's, but it's not specfically stated anywhere.
Thanks,
Bill