This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB to Serial Module (FT232) with Beaglebone black Host mode

Hello

My android compile from this link http://processors.wiki.ti.com/index.php/TI-Android-JB-4.2.2-DevKit-4.1.1_DeveloperGuide and i want to connect my BBB with USB to Serial Module via USB host on my BBB.

I try to configure kernel by enable Device Drivers->USB Support->USB serial converter support->FTDI Single port but that still not working, Please help

Thank you.

  • What is the log you are getting in terminal while you plugging your FTDI module into BBB ?

    May be you happened to mistake while building linux kernel with FTDI driver. after menuconfig if you run the defaultconfig command it will overwrite your old menuconfig hence your FTDI config will lose. 

    Make sure that FTDI is enable in /kernel/.config before you issuing the make uimage- command 

    Cheers

    Sangly

  • Hi,

    Did you get the USB to Serial connection on the BBB running Android JB to work?

    I am trying to do a similar thing. I have compiled Richard Nelson's kernel with the USB support and used Andrew Henderson's pre-built image. I have a USB hub plugged into the BBB. The mouse & keyboard work fine but not my USB to Serial cable. I am porting an existing Android app to the BBB.

    Any suggestions are greatly appreciated.

    Thanks, Suzanne