Hi All,
My device has an existing jffs2 fileystem and it was running 2.6.10 kernel. I am in the process of upgrading the device and I was able to upgrade the kernel image. But, when I boot it, the kernel was throwing an ECC error.
mtd->read(0x400 bytes from 0x22c000) returned ECC error
Seems, the way the kernel 2.610 writes the jffs2 filesystem was not compatible to the latest kernel.
Is there a way to fix this problem?
Thanks,
john