Hello,
I'm having problems getting my C5515 eZDSP USB Stick to initialize. I followed the steps in the Quick Start guide for installation and making a new target configuration, but the problem occurs when I try to "Connect to Target". I get the error:
"Error connecting to the target: Error 0x80000240/-151 Fatal Error during: Initialization, OCS"
On the TI wiki page, I found that this probably means the EEPROM is incorrectly programmed, and I followed the steps to see what VID/PID is actually programmed in the device by checking the device properties in the device manager. The VID/PID programmed is:
VID_0403 PID 6010
This is wrong, according to the wiki page:
http://processors.wiki.ti.com/index.php/XDS100#How_to_make_an_XDS100_.2F_How_to_build_an_XDS100_hardware_emulator
Apparently, it should be VID=0403 PID=A6D0. There is a FTDI utility called MProg with a .ept file referenced on the page that can be used to re-program the XDS100. I downloaded both, but this is where I got stuck. When I scan for devices in MProg, it finds my device and says it is "blank":
I erased just to make sure, but when I try to program it, I get the error:
I've tried uninstalling the drivers for the C5515 eZDSP USB Stick and letting them re-install as I plug the device back in, but that didn't work. The device seems to be working fine because the blinking light demo runs when I plug it in. Am I correct in assuming the problem is the incorrectly programmed EEPROM? Is there anything else I can try? Or should I simply return the device to TI?
I should mention that I am running Windows 8 64 bit and CCS 4.1 (which came on the disk).
Any help would be greatly appreciated!
- Rystian