Other Parts Discussed in Thread: AM3352
HI
I am trying to Interface TiWi5 module with MMC2 on AM3352 based custom board, which is not successful.Earlier i had tried MMC1 with TiWi5 in beagle bone without much issues.
MMC2 is not able to initialize the module.I can see clock and command but no response from tiWi5 module.
I could see the clock of 400KHz in SDIO_CLK and some data on SDIO_CMD. I could not see any data (voltage transition) on irq and SDIO lines.
In few threads i found MMC2 can operate only in 1.8V .Can anybody confirm on that .TiWi5 module uses 1.8V and we have put voltage translator between processor which uses 3.3V
How can i debug the interface ?
I have attached the logs for reference.
Sunil kottary