I have Pandaboard ES Rev B2 and running Android 4.0 (AOSP). I try to do below jobs to switch pin UART4_RX to gpio155 'output' mode3, but it could not working, Why? (PS. If I try to setup it to be input gpio mode3 (0x11b), it will work properly, but could not work for input gpio mode3.)
cd /sys/kernel/debug/omap_mux
sudo echo 0x01b > uart4_rx
sudo cat uart4_rx
name: uart4_rx.uart4_rx (0x4a10015c/0x15c = 0x4100), b ag20, t NA
mode: OMAP_PIN_INPUT | OMAP_PIN_OFF_WAKEUPENABLE | OMAP_MUX_MODE0
signals: uart4_rx | sdmmc4_dat2 | kpd_row8 | gpio_155 | NA | NA | NA | safe_mode