I have Pandaboard ES Rev B2 and running Android 4.0 (AOSP). I try to do below command to show settings of i2c4, its default setting is for mode0 (I2C mode) and PIN_INPUT and not do any internal pull up or down. But I found that its (I2C4_SCL and I2C4_SDA) voltages will always be Hight level 1.8V, Why? (PS. Do not add any external pull up resistor there.) How could I make it to be low voltage (release the bus) in default?
cd /sys/kernel/debug/omap_mux
sudo cat i2c4_scl
name: i2c4_scl.i2c4_scl (0x4a10012e/0x12e = 0x0100), b ag21, t NA
mode: OMAP_PIN_INPUT | OMAP_MUX_MODE0
signals: i2c4_scl | NA | NA | gpio_132 | NA | NA | NA | safe_mode