Hi,
I have a question about AM335x.
I'm searching for NAND spec which AM335x GPMC support.
In AM335x Technical Reference Manual(spruh73j) page.264
" 7.1.1.1 GPMC Features", it's written as follow:
////////////////////////////////////////////////////////////
Up to 16-bit ECC support for NAND flash using BCH code (t=4, 8 or 16) or Hamming code for 8-bit or
16-bit NAND-flash, organized with page size of 512 bytes, 1K bytes, or more.
///////////////////////////////////////////////////////////
What is the max page size and the max block size of NAND supported in GPMC?
best regards,
g.f.