This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Video capturing in DM8148 EVM at lower resolution

Other Parts Discussed in Thread: TVP7002

Hi,

I am using the DM8148 EVM and I want to capture video at 720x576i at 60 fps through the VIP port. I am having the following query

1) Do I need to modify the VPSS firmware to capture enable capturing at 720x576i?  If no then will the VPSS support all standard  resolution up to 1920x1080p?

2) In the TI81XX PSP 04.04.00.02 there is a loop-back application saLoopBack in src/example/video, can that application be used for loop-back at 720x576i?

Regards,

Debasish