I'm trying to build the UBL for DM6467 (for the faster 6467 "T" part number). The help page (http://wiki.tiprocessors.com/index.php/DM6467_EVM_Installation) says to use CCS 3.3 with Perl version 5.10. When I install CCS 3.3 it says it is compatible with ActiveState version 5.6 or 5.8 only. Which Perl version is realy needed?
Also, must the Perl software be from ActiveState? I can no longer get that version from ActiveState for free.
In the past I used DM646x_FlashAndBootUtils_1_50, which I can compile via Cygwin. However, I'm not sure what things need to be changed for the faster "T" part.