This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Beaglebone black

Hi experts,
i am new to this area,
I am using amstrong 3.8.13 kernel in BBB
at first i loaded the device tree as below,
 
 echo cape-bone-iio > /sys/devices/bone_capemgr.*/slots
 
then i used analog pins however i am getting the fixed values that is values are not varying continously as i vary input analog voltage
 
if i go to this path
/sys/devices/ocp.2/44e0d000.tscadc/tiadc/iio:device0
 
and then ls -al gives me
 
total 0
drwxr-xr-x 3 root root    0 Jan  1 03:24 .
drwxr-xr-x 4 root root    0 Jan  1 03:24 ..
-r--r--r-- 1 root root 4096 Jan  1 03:27 dev
-rw-r--r-- 1 root root 4096 Jan  1 03:27 in_voltage0_raw
-rw-r--r-- 1 root root 4096 Jan  1 03:27 in_voltage1_raw
-rw-r--r-- 1 root root 4096 Jan  1 03:27 in_voltage2_raw
-rw-r--r-- 1 root root 4096 Jan  1 03:27 in_voltage3_raw
-rw-r--r-- 1 root root 4096 Jan  1 03:27 in_voltage4_raw
-rw-r--r-- 1 root root 4096 Jan  1 03:27 in_voltage5_raw
-rw-r--r-- 1 root root 4096 Jan  1 03:27 in_voltage6_raw
-rw-r--r-- 1 root root 4096 Jan  1 03:27 in_voltage7_raw
-r--r--r-- 1 root root 4096 Jan  1 03:25 name
drwxr-xr-x 2 root root    0 Jan  1 03:27 power
lrwxrwxrwx 1 root root    0 Jan  1 03:27 subsystem -> ../../../../../bus/iio
-rw-r--r-- 1 root root 4096 Jan  1 03:24 uevent
 
there is no mode directory and buffer directory in list . please help to configure ADC In continous mode.