This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Booting issues with AM335x using XIP parallel flash in 16-bit mode

CPU is unable to start from a XIP (parallel flash) set as 16 bit mode. We are not using parallel flash (and not planning on using….) but when debugging the boot-up I had the CPU being stuck in accessing the XIP in 16bit mode (the CPU does pull down the CS0 but no CLK is provided out ???!!!) Would you be able to help?