This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

QMSS Linking



Hi 

I have a scenario for Infrastructure packet DMA transfer on which I need clarity.
I have a Completion Q on TX side with 100 desc.
I pop a descriptor (DESC 1) and push it to FDQ.
I pop another descriptor(DESC 2) and push it to FDQ.

Now to DESC 1 , I link a descriptor which is also popped from completion queue.
Now to DESC 2.  I link a descriptor which is also popped from completion queue.

Now  I pop from Tx FDQ and trigger the DMA by pushing to TX Q.

Is the scenario ok ?
Because i can see in Tx completion queue, the linked descriptors are not recycled.

Regards

Rahul