This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

how to connect ADC ADS4219 to C66X DSP ?

Hi,

     I want to capture 3 channel 200MHZ signal,  each channel is 10 or 12 bit.  I would like to use three ADS4218 or ADS4219.

     How can I connect the ADS4219 to C6657 or other DSP chip direct ? I don't want to use a FPGA

     I see the UPP max is 75MHZ , it can not fixed.  would you please give me some adivce ? 

     Thanks very much.

  • Hi,

    I don't have any information on the ADS4219. The C6657 doesn't have an interface that can handle those data rates with the exception of the SerDes interfaces like SRIO or PCIE. If the ADS4219 supports either of these then you might be able to connect directly. Typically an FPGA is used to interface with these types of devices.

    Regards, Bill