Hello,TIer.
We wanna use USB of DM8168 in host mode.We connect USB of DM8168 to a usb-hub chip to get file from u-disk which is connected with the usb-hub.
usb(dm8168)<------------->usb_hub<------------>u-disk*4
But,right now,case1:DM8168CCYG4,DVRRDK 3.0
1> Don't connect usb_hub to dm8168's usb before power up the system.
2> Power up the system,;
3> Connect usb_hub to dm8168's usb port,
The result is that DM8168 cannot recognize the usb_hub.But if we change usb_hub to usb-disk,the result is different-----DM8168 can recognize the usb-disk for hotplug.
What may cause the problem?