This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Short time Fourier transform library function ?



Hello all,

Quick question:

I just wondered if there was short time Fourier transform function that someone has written that would be suitable for the 6713 DSK ?

Many thanks,

Jack 

  • Hi Jack,

    Thanks for your post.

    I believe, there are some FFT examples demonstrates the use of the C67x DSPLIB FFT filtering capabilities

     and performance benchmarks referred in the below E2E thread:

    http://e2e.ti.com/support/dsp/tms320c6000_high_performance_dsps/f/115/t/265955.aspx

    Also, there are sample code available in the above thread (0815.fft_example_sp.c & 5238.fft_example_sp_spra947a.c)

    Thanks & regards,
    Sivaraj K

    ------------------------------------------------------------------------------------------------------- 
    Please click the Verify Answer button on this post if it answers your question.
    --------------------------------------------------------------------------------------------------------

     

  • Sivaraj, many thanks for the reply,

    I was rather hoping there was a library function for the STFT, I am currently using a similar FFT function in a loop-like manner to go through my time domain signal and calculate the STFT. It's a bit temperamental so I was hoping there was something a little bit more robust.

    Thanks,
    Jack