This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

powervr driver on /dev/fb1

Guru 10685 points


I've got some Qt graphics running using the powervr driver and the graphics are on /dev/fb0.

1) How do I get the graphics to appear on /dev/fb1 instead?

2) Is there any way to reorder the framebuffers so fb0 appears on top of fb1 for instance?

In case you're wondering, I need this because of the way I am mixing framebuffers.

Thanks,

Ralph