Other Parts Discussed in Thread: AM3359
Hello,
I was given a SBC8600B board, featuring a AM335x processor. The problem is that the flash was somehow erased, and now It is not possible to boot neither linux, android or WINCE700.
Basically, on the serial terminal it is never displayed the u-boot prompt, but only a sequence of "CCCCCCCC" characters. I also tried to use "starterware" to send .bin files, and those are excecuted (by uart, not SD), but I wonder if there is a possibility to copy a linux image (boot.img) to try to recover the FLASH.
The SDcard is useless since it is not recognized, I cannot even use it with the files from starterware.
Thanks in advance.. I would really appreciate some help with this issue :D