Hello,
I got an AM3359 on a beaglebone black (Master) and try to talk to a CC1200 (Slave) via SPI. To start a conversation I set the chip select manual to active (low) and if the CC1200 is ready for conversation it also set the MISO to low (this process I can see on my oscilloscope). To check this I have to read the input level of MISO Pin but I cannot find a way to do this.
I already tried to mux the pin to a GPIO and get the value of DATAIN register but that stop the connection to CC1200.
I look for something like: while( HWREG("Register on am3359") & MISO_INPUT_BIT ); to wait till MISO goes low.
thanks for replies
Robert
Edit: I try to use the SPIDAT_0 Bit in MCSPI_SYST register but this works only if I set the SYSTEM_TEST Bit in MCSPI_MODULCTRL. While doing this the Transmission stops.
Is it possible to check the MISO state with MCSPI_SYST Value or have I done something wrong?