Other Parts Discussed in Thread: OMAP-L138, OMAPL138
Hi there,
I'm currently working with the OMAP-L138 Kit from LogicPD and try to run the uPP.
I want to use the example upp_DSP/BIOS_driver code from the davincidsp wiki-page. I just changed into transmit mode and tried to capture the data.
But when I run the program the upp_interrupt_cout is never increased, and thus it gets stuck in line 206.
I get also 2 Errors when I start CCS3.3 because it can't find the 2 GEL files OMAPL138_DSP.gel and OMAPL138_ARM.gel. But I think it should be negligible, as it says that the initialisation doesn't rely on GEL.
Is there an update for this example code? Or anyone had encoutered this problem as well?
It is my first programming project, so a working example would help me a lot! Thanks!
Best Regards,
Michael