For those interested I have a new site on Codeplex supporting Windows Embedded Compact 7 on the BeagleBone:
https://beaglebonebsp.codeplex.com/
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
For those interested I have a new site on Codeplex supporting Windows Embedded Compact 7 on the BeagleBone:
https://beaglebonebsp.codeplex.com/
Dear DavidVescovi,
I have downloaded the image your mentioned. I have loaded a 4GB SD card with the MLO, EBOOTSD.nb0 and NK.bin that comes with the Demo package, Also I have formatted the card with Fat32 and 4096 byte sectors (using hp format tool), and I have used the TI SD card utility for flashing the SD card, Also I have pushed the user button before power up, But noting happens!!!
In some procedure they said to format using hp format tool, copy mlo,ebootsd,nk.bin in correct order But but not booting...
when I power the board up the leds won't flash, , So I think it's a boot problem, How can I be sure that the MLO is in the first sector of the SD card?
I have loaded and booted angstrom img succsfuly on BeagleBone Black.
I am using 4gb sd card, windows 7 and virtual machine xp.
so please help me to find this issue.
Regards
aswin pp
The image works just fine. Recheck your procedure.
Format uSD card with HP tool. Copy MLO file to card, then ebootsd.nb0 and NK.bin.
Hold user button (the one in the back near USB host connector)) down while powering up unit.
Release button and it should boot.
Hi DavidVescovi,
Thank you for replying. The same image not working for me, i thought that the problem on sd card.
Did you know the procedure to make sd card bootable and copying nk.bin, mlo, ebootsd files.
I already tried hp format tool, pls reply...
Hi DavidVescovi ,
Thank you for replying.
please just send me the procedure to make bootable sd card.
hi DavidVescovi
what the means of only 4th LED fluctuation at boot time by SD card ??????
how can we check that booting is going on or not??????
please reply........thank
hook up the debug console. Configure serial port for 115200 baud, use HyperTerminal or Teraterm.
You will see messages on console as booting progresses.
hi DavidVescovi,
I don't have serial converter for bbb. I am trying to boot from sd card. Is there have any other method other than serial debugging.
If you followed directions closely and properly formatted card, copied files and hold user button down while powering on it will boot. Note: It may take 15 or so seconds to load. If it is not you will have to debug to see what you did wrong.
by using minicom i got this out put
============================================
Welcome to minicom 2.5
OPTIONS: I18n
Compiled on May 2 2011, 10:05:24.
Port /dev/ttyUSB0
Press CTRL-A Z for help on special keys
CLIENTCLIENTCLIENTCLIENTCLIENTCLIENTCLIENTCLIENT
========================================================
I think image i fine ,i had not got any garbage data but whatever I got what is the mean of this.......please help me THANK YOU