This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

H264: 2 x Super High Definition

Hello,

Could anyone please confirm that the Ti's H.264 can encode 2 super high definition streams i.e. 2560x1600 (x2)? If not, then what are the limitations?

I am using the dm816 on SDK 5_04_00_11.

kalex

  • Processor can perform a single 1080p60 H.264 encode or decode or multiple lower resolution or frame rate encodes and decodes. Multichannel HD-to-HD or HD-to-SD transcoding along with multi-coding are also possible. With the ability to simultaneously process 1080p60 streams.