Other Parts Discussed in Thread: SYSBIOS
Hi,
I wish to enable L2 cache at startup to its maximum using XDC script.
Also Please try to give the code if it is done in the code.
regards,
Sijomon
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: SYSBIOS
Hi,
I wish to enable L2 cache at startup to its maximum using XDC script.
Also Please try to give the code if it is done in the code.
regards,
Sijomon
Sijomon,
What version of SYS/BIOS are you using?
have you tried adding var Cache = xdc.useModule('ti.sysbios.family.c66.Cache'); into your .cfg file?
SYS/BIOS Version 6.35.1.29
In my platform file I have set L2SRAM in cache mode.
What I read from the SYS/BIOS manual is that if it is done so, then the XDC will do the necessary to setup L2PCFG in order to make it work as cache. But it is seen that this register is not set. Then I had to write the code for changing it cache and plugged it as start-up function. Then everything was fine. What I wish to know is that, whether will it be automatically taken care if enabled .If not, is it possible to do it in the XDC Script?. Then what is that script?
Doing via C code has been experimented.
instead of calling c66.cache module, would hal.cache be sufficient for this purpose? Anyway that was also done. Still L2PCFG was not setup.
regards,
Sijomon
Hi Sijomon,
This is working fine on my evm6678 board. I created my own platform, set the L2 Cache to "512K" and when I run the program and it gets to main(), the cache L2CFG shows the LSB as a 0x5 which means it is "512K"
Make sure nothing else is coming by to overwrite this info in your program.
Judah
Hi,
I'm pretty sure one of the other packages that you are using must be overriding the Cache settings.
One thing to try if you can is use a Hardware watchpoint of the cache L2 cfg address 0x01840000 to see what software packages are writing the cache bits.
If you still can't figure it out make a cut down version of your program that reproduces the problem and attach it here and I can try it on my end.
Judah