- I installed a branch to softwareDispatch at the SWI vector #8.
- When SWI #0x1 is called it jumps to 0x08 as I expected and CPSR mode = 0b10011 ( supervisor )
- Why does the branch instruction EA00007C jump very far to location 020007e4?
- I expected it to jump to softwareDispatch @ 00000200
Here is what it looks like as I single-step through the debugger:
=>800028f0: EF000001 SWI #0x1 ... ... ... 00000000: EF3D7039 SWI #0x3D7039 00000004: C8D346BE LDMGTFD R3, {R1-R5, R7, R9-R10, R14}^ =>00000008: EA00007C B softwareDispatch 0000000c: 8ABD2FBC BHI 0xFEF4BF04 00000010: 0E439F7D MCREQ P15, #0x2, R9, C3, C13, #0x3 00000014: D589E967 STRLE R14, [R9, #0x967] 00000018: 9A17D020 BLS 0x005F40A0 0000001c: 82CF6450 SBCHI R6, PC, #0x50000000 ... ... ... =>020007e4: E2877002 ADD R7, R7, #0x2 020007e8: E3550009 CMP R5, #0x9 020007ec: 8A00000B BHI 0x02000820 020007f0: E28FC000 ADD R12, PC, #0x0 020007f4: E79CF105 LDR PC, [R12, R5, LSL #2] 020007f8: 0200098C ANDEQ R0, R0, #0x230000 020007fc: 02000950 ANDEQ R0, R0, #0x140000 02000800: 02000914 ANDEQ R0, R0, #0x50000 ... ...
I expected the branch instuction EA00007C to end up here @ 0x200. What happened?
57 void softwareDispatch(int softwareInterruptNumber, uint32_t * regs) { softwareDispatch: =>00000200: E92D400E STMFD R13!, {R1-R3, R14} 00000204: E58D1004 STR R1, [R13, #0x4] 00000208: E58D0000 STR R0, [R13] 63 asm(" nop"); label1: 0000020c: E1A00000 MOV R0, R0
My eventual goal is to switch to supervisor mode so I can enable ARM interrupts in CPSR.
/// Updates contents of 'vector' to contain branch instruction /// to reach 'routine' from 'vector'. Function return value is /// original contents of 'vector'. /// NB: 'Routine' must be within range of 32MB from 'vector'. /// /// Usage: /// \code /// unsigned *irqvec = (unsigned *)0x18; /// Install_Handler ((unsigned)IRQHandler, irqvec); /// \endcode /// /// \remarks routine must be located within 32Mbtes of the vector unsigned installHandler(unsigned routine, unsigned *vector) { unsigned oldvector; // routine is the pointer point to the IRQ handler. // shift right 2 is for address word aligned. // subtract 8 is due to the pipeline // since PC will be fetching the 2nd instruction // after the instruction currently being executed. unsigned newVector = ((routine - (unsigned) vector - 8) >> 2); if (newVector & 0xff000000) { printf("*** Error handler greater than 32MBytes from vector\n"); return 0; } // to implement the instruction B <address> // 0xea is the Branch operation for "branch always" (BAL) newVector = 0xea000000 | newVector; oldvector = *vector; *vector = newVector; return oldvector; }
// Install the softwareInterruptDispatcher so we cchange modes to enable interrupts unsigned *irqSwiVector = (unsigned *) (8); unsigned softwareInterruptHandlerFunctionPointer = (unsigned) softwareDispatch; oldVector = installHandler(softwareInterruptHandlerFunctionPointer, irqSwiVector);
-Ed
CCS v5.5
DM6446