This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

use camera sensor with dsplink, cmem, etc

Other Parts Discussed in Thread: DM3730

Hello,

I'm using dm3730 processor along with a ov3640 camera sensor. I'm working with the ti-dvsdk_dm3730-evm_04_03_00_06 and the appropriate 2.6.37 linux kernel. With a working camera driver I'm able to grab images and store them to memory. My goal is to use some kind of a image processing algorithm on the dsp from with the image I stored in memory. So for that I read that the sdk provides the dsplink, the cmem and the lpm driver to work with the dsp, but I don't really understand the need of the codec engine.

Would you recommend me to use the codec engine or are the other drivers sufficient?

Are there already some tutorials with that task?

Best Regards, Tom