Hi everybody,
I've been working on a beaglebone clone board which is not executing OS, app or any code supposed to be located from 0x80000000 onwards.
I've saw a post at google groups where an user says:
"If you do not clone it EXACTLY, PCB layout. then you have to run special SW using Code Compose Studio to calculate the DDR timings. They are different if you change the routing on the DDR."
If this information is right, could somebody point me to this "special software" in order to "calculate" DDR timings? Although it's a clone, perhaps little diferences in pcb routing or manufacturing could be causing the problem.
Furthermore, is there any way to check if memory is working at least?
I'm using CCS 5.5.0, XDS100v2 (FT2232H), and AM335X_StarterWare_02_00_01_01.
Bootloader, *.ccxml and GEL files are ok since I can run them on a original beaglebone.
Thanks,
Victor Leite