This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335X Graphics SDK openembedded recipe available

Hi All, 

   I am trying to use the X11 libraries provided with the Graphics SDK along with the libraries provided in the rfs of the Sitara SDK. However when I try to link a program using these libraries, the loader fails to load the X11 libraries.

As a possible workaround, I was trying to go back and rebuild the prerequisite pieces ie. kernel, and rfs from PSP_04.06.00.10 Release. I am looking around for the root file system that accompanies this PSP release, but I am having some trouble locating it. Can anyone point me in the right direction. I am hoping for an oe recipe that will allow me to download and compile the rfs components. 

Also, is there an oe recipe that would allow to download and build all the requisite components that make up the Graphics SDK (esp the source that yeilds the X11 libraries ) 

Thanks Much 

Victor