This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3358BZCZ100 PROCESSOR analog input

I am using the AM3358BZCZ100 PROCESSOR. I would like to confirm that the input analog voltage range is 0-1.8V when the processor is powered 3.3V. Also do I need input protection on these pins while the processor is not powered. Thanks

  • Hi hj,

    The analog pins of AM335x (ADC) are powered from VDDA_ADC power input. The voltage that can be applied there is 1.8V. 

    The measurement range depends of the voltages applied to pins VREFN and VREFP and cannot be greater than VDDA_ADC (1.8V). See AM335x Datasheet Rev. F, Section 3.5 Touchscreen Controller and Analog-to-Digital Subsystem Electrical Parameters.

    BR,

    Vidin

  • On your second question, yes, you need protection. The AM335X I/O pins are not fail-safe and no voltage should be applied to them before the processor power supplies have ramped-up and stabilized. Check AM335X Datasheet Rev. F Table 3-1, parameter "Steady State Max. Voltage at all IO pins" and Note 8 after the table.

  • You should never apply a voltage potential that is greater than the respective supply voltage for any terminal that is not fail-safe.

    USB0_VBUS and USB1_VBUS are the only fail-safe terminals on AM335x.  Therefore, you must not apply any potential to the analog inputs when the device is powered off.

    This requirement should be applied for all conditions, power-off, power-up, power-on, and power-down.

    Regards,
    Paul