Greetings E2E.
What is the maximum frequency we can clock data out and read data in – one page in data sheet says max 100MHz – can this figure be confirmed?
Thanksi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Greetings E2E.
What is the maximum frequency we can clock data out and read data in – one page in data sheet says max 100MHz – can this figure be confirmed?
Thanksi
No (partly). I thing you refer to "spruh73g.pdf".
I'm using an AM335X quite a time (Starterware on BeagleBone White) and now i know:
100 MHz is the standart io-clock and has nothing to do with the real IO-Performance.
Using the A8 core, there are 4 busses between core and output, around 10 - 15 MHz Pinwrite is achievable.
Reading pins is significantly slower (using the A8 core). Reading a pin triggers a pin-sampling (adjustable 2-3 clocks) and goes 2 times through the 4 busses (reading needs a request, writing a pin is "fire and forget").
BUT! : Using the PRUSS-ICSS, some people mentioned that they achieved 200 MHz writing IOs, and in some PRUSS-ICSS slides (sorry, i don't know the actual source, it's a TI-document) there is a 16 bit + clock Input diagram, where the input is (2x chained) sampled with 200 MHz.
I can not confirm the PRUSS-ICSS performance, because i don't know how to program the AM335x with Starterware AND one of the two PRUSS-Cores (M3, i think).
(Please, i want outstanding Performance with the Beaglebone. Therefore dear TI-developers, how can i use the PRUSS-Cores with Bare-Metal-Programming?)
I hope this helps (if you are using an AM335x). Greetings
Martin Boeckler
Thanks Biser for the hint.
First: I should update my resources.
Second: Regarding the PRUSS i will investigate the possibilities, thanks.
Additional:
For Bitbanging, the PRUSS sounds good. But for high input/output data Rates, the Input datatransfer is limited because of the needed PRUSS-Code. (http://e2e.ti.com/support/arm/sitara_arm/f/791/t/149413.aspx)
For high data throughput, the gpmc interface sounds good. (http://e2e.ti.com/support/arm/sitara_arm/f/791/t/312694.aspx)
Greetings
Martin
Hi Martin B,
would you please let us know how you achieved a GPIO output rate of 10 to 15MHz?
I only got 1.136MHz for an on/off GPIO output with a signal that was not equidistant. (See http://e2e.ti.com/support/embedded/starterware/f/790/t/366081.aspx)
Thank you!
Martin H.