Hi,
I am using OMAP 3530. Using DSPLink I am able to load and unload DSP.
I have 2 sample DSP .out files. (DSP1.out and DSP2.out). If i load and unload any one of the out files (either DSP1.out or DSP2.out) continuously each will work fine but when I load DSP1.out then unload and then try to load DSP2.out its causing trouble. Sometimes its showing "DSP MMU Error Fault! MMU_IRQSTATUS = [0x1]. Virtual DSP addr reference that generated the interrupt = [0xff114060]." Error
Sometimes the linux kernel hangs and the serial console becomes unresponsive. Why is this happening? Please help to fix this problem
regards
Vishu